Wanting to know if we can run as an AP and a STA simultaneously. Since it (looks like) we can only support one 'incoming' connection to an AP, I am optimistic.
p2p won't work, sadly.
-Dave
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Dave,
I'll separate your post to several topics:
Thanks,
Alon
Alon,
I have been pursuing using the CC3100 chip in a new product and I have just now become aware that only one STA connection is permitted in AP mode. This will not work for me as my application requires up to 5 simultaneous connections.
You mention that more connections will be supported in the near future. Can you elaborate on the timeframe for this and the number of connections that may be allowed? I need to decide if I should abandon the CC3100 and pursue another chip or if it will be upgraded soon enough to allow me to use it.
Thanks much,
Aaron
Aaron,
Unfortunately, we don't have any firm plans to support 5 simultaneous connections.
Adnan
Hi,
No progress in this topic. No multiple AP clients, no simultaneous STA + AP. I expect that this features will be never implemented CC3100 and CC3200. Network processor haven't sufficient resources for this features.
Jan
gentlemen - have you read the CC3200 data sheet, first page? i realize this is an older post you have revived, but we do have enough serious posts to deal with. also, we do have WL187x devices if you need more capability
thanks! and let us know if this is still not what you expected.
This are good question. Am not able answer it.
I haven't available official statement in this case, but according "answers" from TI employees at E2E forum and other confidential information, I am almost 100% sure. Unfortunately I can't share more information.