Hi team,
I have couple questions regarding our CC3200:
1. Do we support beacon and DTIM skipping?
2. We have an Apple WAC method MFI chip, is the WAC/MFI implemented on our CC3200?
Best regards,
Max
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Max,
Regarding Beacon and DTIM skipping, It is supported in CC3200 Firmware in Low power mode.
Note that It works in client mode only. Also it automatically terminates mDNS service and internal HTTP Server. Application initiated UDP/TCP Server will see unpredictable system behavior.
Regards,
Kaushal
Max
You can find more information on Network Sub System Programmer's Guide.Refer to Section, 4.6.1
http://www.ti.com/lit/ug/swru368/swru368.pdf
Regards,
Kaushal
Max,
Regarding WAC, it is supported by CC3200.
Detailed information about the WAC feature is available to Apple MFi Development and Manufacturing licensees.
The SimpleLink Wi-Fi CC3100 and CC3200 platforms provide customers the most flexibility with provisioning
methods, you can find additional details in this White Paper:
http://www.ti.com/general/docs/lit/getliterature.tsp?baseLiteratureNumber=swry011&fileType=pdf
Adnan
Hi Max,
If your query is answered. Please check verify answer.
Let us know if you have any more query.
Is the DTIM skipping supported in the CC3100 as well?
If yes, how do I enable it? (SDK v0.5.2)
Can I set how many DTIMs to skip between each listen?
Thanks,
Nir