Hi,
I would like to implement the uPnP (Universal Plug-and-Play) Protocol over the TCP/IP Stack that comes with the TI-RTOS in the CC3000 Modules.
I have a library (C-file) which works perfectly with the standard Linux-based TCP/IP Stacks (which use standard sockets for interface).
Can I use the same library file to interface to the TCP/IP Stack present in the TI-RTOS?
Is there any example projects for the same.
Thank you.
Regards,
Abhay