Hello, I am a beginner in this field.
My requirement is to transfer a bmp image from PC to the custom PCB over Wi-Fi which has CC3100 in it. The FPGA connected to the SPI port of CC3100 must read the image as and when it is available.
But before making the PCB, I would want to try this using any available evaluation boards.
My questions are :
1. Is it possible to do what I am planning, with the chip?
2. Evaluation board which has CC3100 with antenna connections and SPI pins available for external connection?
3. Any software application from TI is available to send the bmp image (or any data) from PC to CC3100 over Wi-Fi?
4. How do I configure CC3100 for my requirement, I don't see any register settings in the datasheet? OR I don't need to do any thing and just use it?
As far as possible, I would like my evaluation set-up to be closely resembling the actual one. So I would prefer evaluation boards which has only CC3100 and not many of TI micro controllers as I don't use them in final set-up.
I would greatly appreciate any help regarding this.
Thanks,
Vinayak