Hi,
I'm using the cc3200 launch pad and testing the wlan_station project (from the CC3200sdk v0.52). The output from TeraTerm when running is like so:
************************************************* CC3200 WLAN STATION Application*************************************************
Host Driver Version: 0.0.5.1
Build Version 2.0.7.0.31.0.0.4.2.1.5.3.3
Device is configured in default state
Device started as STATION
[WLAN EVENT] STA Connected to the AP: Home ,BSSID: x:xx:xx:xx:xx:xx
It hangs here and never displays that an IP is acquired like so:
[NETAPP EVENT] IP Acquired: IP=192.168.1.116 , Gateway=192.168.1.254
When I've tried wlan_station on other routers, it has worked. It's only failing to acquire an IP address on my home router. I've tried rebooting router, confirmed that security setting, SSID, and password are correct. Other devices like MacBooks, PCs, and iPhone's can connect to the router fine.
What should I do to debug, considering it's only failing on this specific router?