Hi,
Anyone here have made the Exosite Cloud Demo work for CC3200 Launchpad? I am following the steps from the link below and seem that I failed download of binary file as I have an error message at the end of the Uniflash log.
https://support.exosite.com/hc/en-us/articles/202271424--CC3200-Wi-Fi-Launchpad
Uniflash Log:
[19:39:01] INFO: > Executing Operation: Disconnect
[19:39:01] Operation Program returned.
[19:39:14] Begin Program operation.
[19:39:14] INFO: > Executing Operation: Connect
[19:39:16] INFO: setting break signal
[19:39:16] INFO: --- please restart the device ---
[19:39:20] INFO: connection succeeded
[19:39:20] INFO: getting storage list
[19:39:20] INFO: > Executing Operation: Init
[19:39:20] INFO: reading version info
[19:39:20] INFO: DEVICE CC3200 ES1.32
[19:39:20] INFO: reading version info
[19:39:22] INFO: reading version info
[19:39:22] INFO: reading version info
[19:39:24] INFO: > Executing Operation: Program
[19:39:24] INFO: > File name: /sys/mcuimg.bin, Update: true, Erase: true
[19:39:24] INFO: > Erase File: /sys/mcuimg.bin
[19:39:24] INFO: erasing file "/sys/mcuimg.bin"
[19:39:24] INFO: deleting file "/sys/mcuimg.bin"
[19:39:24] INFO: erase file completed
[19:39:24] INFO: > Size of file = 177624
[19:39:24] INFO: > Update File: /sys/mcuimg.bin
[19:39:24] INFO: Downloading file "/sys/mcuimg.bin" with size 177624
[19:39:24] ERROR: Open operation failed
[19:39:24] INFO: > Executing Operation: Disconnect
[19:39:24] Operation Program returned.
After this I removed the SOP2 Jumper, I followed the instruction below from the link. But, I can't seem to do that using my Iphone4s. Anyone here know what part I am doing wrong.
Using a smartphone, tablet or other wifi device, connect to the mysimplelink-XXXXXX access point. Then open a browser, navigate to http://mysimplelink.net. On the home page, take note of the MAC Address, you'll need it to link the device to your Exosite account. Then, go to the profiles page and select the SSID of the network you'd like to connect to, select the security type, enter the security key if needed, and push "Add".
Your device should now connect to your network and begin communicating with Exosite.
If you do not see the mysimplelink-XXXXXX access point, your device may already have a valid network saved. It force it into AP mode, hold SW3 and tap RESET and wait about 5 seconds, you should now see the access point.
- kel