Hi,
I define CC3200 as AP with HTTP and TCP server capabilities.
I can connect to it with Note 3 and with a laptop, access the embedded web server pages with the browser and
the tcp server with a .Net TCP client application. The data exchange between TCP client and server works well
in both directions.
When my station connects to CC3200, SL_WLAN_STA_CONNECTED_EVENT and SL_NETAPP_IP_LEASED events are received.
There is no other Wifi station set to connect to CC3200.
But sometimes after CC3200 reset, immediately the SL_WLAN_STA_CONNECTED_EVENT (but not also SL_NETAPP_IP_LEASED) is received and pSlWlanEvent->EventData is empty( I've checked with the debugger).
And due to the fact that CC3200 AP can accept only 1 station, of course I cannot connect with my station.
How can I detect who is connecting to the CC3200 AP ?
This is the log of the running sequence :
Manufacturer ID: 0x5449
Device ID: 0x67
Configuration register value: 0x7480
CHIP ID: 0xf8
[NETAPP EVENT] IP Acquired: IP=192.168.1.1 , Gateway=192.168.1.1
Device is in AP Mode, Please Connect to AP [mysimplelink-113DE1] and type [mysimplelink.net] in the browser
TCP server socket created. ID : 16
TCP server socket binded. Status : 16
TCP server socket is listening...
[WLAN EVENT] A station connected to me. // SL_WLAN_STA_CONNECTED_EVENT
Please advise.
Thanks in advance and best regards to all the community,
Sorin.