Hi All,
Question does TI CC Debugger support CC3200?
http://www.ti.com/tool/cc-debugger
if not what is the proper hardware for flashing/debuging CC3200 Typical system like this?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi All,
Question does TI CC Debugger support CC3200?
http://www.ti.com/tool/cc-debugger
if not what is the proper hardware for flashing/debuging CC3200 Typical system like this?
Hi Ali,
Based from the CC Debugger link below, CC3200 is not supported
http://www.ti.com/tool/cc-debugger
From the CC3200 Launchpad Hardware User's Guide below, you can program CC3200 through JTAG pins using XDS100.
http://processors.wiki.ti.com/index.php/XDS100
http://www.ti.com/lit/ug/swru372a/swru372a.pdf
- kel
Hi Markel,
I was wondering if this solution replaces the need for the FTDI & JTAG emu circuit shown in the user guide? That's because I want to make my board as compact as possible, and I was wondering if the FTDI chip is really necessary to flash/debug.
I'm pretty new to all this, but I wasn't able to find a direct answer to what I'm looking for.
Thanks for the help!
-Li-Yen
Yang1 said:I was wondering if the FTDI chip is really necessary to flash/debug.
No, you do not need to include this on your board design. You can use an external programmer, for example you could modify the CC3100 EMU Boost or you could possibly use a FTDI cable for programming. For debugging, you could use a JTAG emulator like the XDS100/200.
So to clarify:-
Programming: This is programming the external serial flash. You would connect to UART pins as described in this link - http://e2e.ti.com/support/wireless_connectivity/f/968/p/353805/1251290.aspx#1251290
Debugging: This is debugging against the CC3200 MCU. You would use a JTAG or SWO emulator for this. Details on the pins and config can be found in the CC3200 TRM - http://www.ti.com/lit/ug/swru367a/swru367a.pdf
I have not done this my self, so if anyone can either clarify or confirm my assumptions, that would be good.
Glenn.