I've been able modify the http server example for my needs and load my webpages with the uniflash tool. I've looked at the information in the wiki about the uniflash tool, but have some questions.
1 - When I initially access my webpage, there is a login that requires "admin" and "admin" for username and password. Where should I make changes to eliminate the login requirement?
2 - I've failed to erase the old files in the serial flash that were for the default application loaded at the factory. My uniflash project looks like this:
I believe that I need to open the correct .ucf file and then select erase for all of the files that were previously loaded. Is this correct and which .ucf file should I open? Is it the "out of box" project?
I see a page with heading shown and when I click the "SimpleLink CC3100" tab it takes me to my page (main.html). I want to remove all of the pages that were previously loaded and only have my html files in the serial flash.
3 - After I've finished my development, what is the correct process for reloading the default application shown above? Would I check erase for the html files for my project's .ucf file and then press program, open the "out of box" .ucf file and program it?
4 - Also, I'm unclear about when it is appropriate to press the Format and Service Pack Update buttons in uniflash?
I'm really impressed with the device and the development tools. TI has put a bunch of thought and work into this.
Thanks for any help.
Matt