Hello all,
I need by a professional advice, because of that I decide to open this post. I have some issues, that I can't find a general solution:
1. In the Technical reference (swau367a) there is a Table 16-12 (Recommended Pin Multiplexing Configuration). In this table are listed different configurations about how to be configs IO's of CC3200. If I decide to use one of this configurations (Pinout #4 for example), what changes can be make to use this configuration? Is there any reason this changes to change the lowers levels in the script (files such as driver.c; sipmlelink; ti_rtos_config).
2. What is SoP? What are JTA and SWD used for? Is it important to be used for industrial application, because for now I use only Flash configuration (SOP2)?
3. In Quick Start Manual I see the description that PIN_58 must be connect to VCC to configure CC3200 into Access Point mode using default parameters. How much important is this configuration? In my script I configure CC3200 to default access point parameters, is it necessarily and pin 58 to be connect to VCC also?
4. What is the purpose of M25PX80-VMN6TP? I want to replace it with M25PX32, which is 32Mb external memory. Pinouts are identical on both chips. Is it possible CC3200 to have access to 32Mb address map of M25PX32? Is there any limit of accessing of the external Flash address map?
Sorry about long questions! Thanks in advice :)!!
Best regards,
Sergey Mihaylov.