As part of the process to port libcoap to the CC3200 I have hit a number of obstacles.
The primary problems are related to the absence of IPv6 support and hence the absence of functions such as getaddrinfo() - getnameinfo() - freeaddrinfo() and gai_strerror().
Since developing and integrating these functions represent a significant amount of work (although some examples are available ie http://www.netperf.org/svn/netperf2/trunk/src/missing/getaddrinfo.c ) I would prefer to use the built-in IPv6 support for SimpleLink that I believe will be coming.
Does anybody have an idea when IPv6 support will be available?
Alternatively, has anybody implemented this functionality and would be willing to share it.
Thanks