Hi.
i just received sevral new CC3200 sample chips of which the chip verison is 1.33, and i replaced old v1.21 chip with v1.33 chip on the CC3200 moduel.
i use CC3200SDK_1.0.0 , CC31xx_CC32xx_ServicePack_1.0.0.1 and GCC compiler. everything works fine if i don't add any function related to simple link. if i add simple link function, when calling sl_Start(), CC3200 force itself to keep resetting.
Any help would be appreciated.
Best Regards,
Eugene.