To get CE certification, I need to write ESTI EN 300328 V1.8.1 Document.
could you see three question below this line and please give me the information about each questions.
c) Adaptive / non-adaptive equipment:
□ non-adaptive Equipment
□adaptive Equipment without the possibility to switch to a non-adaptive mode
□adaptive Equipment which can also operate in a non-adaptive mode
d) In case of adaptive equipment:
The Channel Occupancy Time implemented by the equipment: ......... ms
□The equipment has implemented an LBT based DAA mechanism
• In case of equipment using modulation different from FHSS:
□The equipment is Frame Based equipment
□The equipment is Load Based equipment
□The equipment can switch dynamically between Frame Based and Load Based equipment
The CCA time implemented by the equipment: ........ μs
The value q as referred to in clause 4.3.2.5.2.2.2 .........
□The equipment has implemented an non-LBT based DAA mechanism
□The equipment can operate in more than one adaptive mode
e) In case of non-adaptive Equipment:
The maximum RF Output Power (e.i.r.p.): ………. dBm
The maximum (corresponding) Duty Cycle: ………. %
Equipment with dynamic behaviour, that behaviour is described here. (e.g. the different combinations of duty cycle
and corresponding power levels to be declared):
......................................................................................................................................................
......................................................................................................................................................
......................................................................................................................................................
I'm always appriciate for your help.