Hi all,
What is the latency on the CC3200 launchpad and audio booster pack (CC3200-LAUNCHXL + CC3200AUDBOOST) when used to stream wireless audio? I am looking specifically at the demo here: http://processors.wiki.ti.com/index.php/CC32xx_Wifi_Audio_Application
What factors would affect this latency if it is variable (and are strategies available to mitigate it)?
The audio stream does not have to be particularly high quality- it is unidirectional, mono, and could be half the bit-rate of CD quality (44.1kHz) if that improves latency, which is the priority. Ideally, we would like to get it to 2ms, though 4 would be ok. If it is not possible on this platform, are there any suggestions for one that could handle wireless streaming with those latency figures?