New to CC3200 launchpad, we're able to flash in latest service pack and compile and load code, everything works fine with 'getting_started_with_wlan_station' example. So both HW and dev environment seem to be fine.
When trying to build and run the 'p2p' example though, it stuck with the following error, any idea why? Thanks.
*************************************************
CC3200 P2P Demo Application
*************************************************
Scan Wi-FI direct device in your handheld device
Host Driver Version: 1.0.0.1
Build Version 2.0.7.12.31.0.0.4.5.1.5.3.20
Device is configured in default state
Started SimpleLink Device: P2P Mode
Error [-7] at line [920] in function [P2PConfiguration]
Setting P2P configuration failed