Hi,
I'm running the P2P application on the CC3200 with no results. I am using the android SDK example (http://developer.android.com/training/connect-devices-wirelessly/wifi-direct.html import from the SDK in Android Studio or Eclipse). To reproduce:
- Turn off wifi on Nexus 3 or 5
- Turn on wifi
- Run Android WiFi Direct application and begin search
- run p2p application on CC3200
- After terminal attached to CC3200 shows "Connect to cc3200-p2p-device"
- In p2p application the STATUS_BIT_P2P_DEV_FOUND goes true
- shows up as Peer under Android application
- Hit connect on the Android device
- Everything hangs here
The simple link layer never sets the STATUS_BIT_P2P_REQ_RECEIVED.
Does anyone have a list of devices that the p2p program proved stable on? Can anyone provide more information on debugging the P2P portion using a debuggable Android platform?
Thanks,
j