Hi Everyone,
I set up CC3100 to AP mode, 3 tcp/ip servers: listen to port #23, #80, and #8080.
the host application call sl_accept to establish new connection and sl_close to close the client socket ID.
I have been using Teraterm and wrote a Teraterm macro script to test the connection and disconnection. First client connect to port 8080, pause 250ms, disconnect, pause 250ms; secondly client connect to port #80, pause 250ms, disconnect, pause 250ms; Finaly client connect to port #23, pause 250ms, disconnect, pause 250ms. Then repeat the cycle.
The issue is the test runs for about 15 minutes then Host MCU reset.
Here is the Teraterm macro script:
while 1
connect '192.168.0.1:8080'
mpause 250
disconnect 0
mpause 250
connect '192.168.0.1:80'
mpause 250
disconnect 0
mpause 250
connect '192.168.0.1:23'
mpause 250
disconnect 0
mpause 250
endwhile
CC3100 has ip address of: 192.168.0.1, client has ip address of 192.168.0.100.
Why CC3100 caused the host to reset?
Thanks,
Dennis