Hi,
I am designing a board with CC3100MOD .
I understood that I can choose between UART and SPI.I mean, the communication is UART or SPI, I don't need both of them?
If that True, can you explain to me what is mean?
http://e2e.ti.com/support/wireless_connectivity/f/968/p/382900/1354320.aspx#1354320
Is the serial flash on the CC3100MOD not preformattet you mean?
It was my mistake, I missed that you are using the module here. All the module are pre formatted and service is updated.
But you should still route the UART pins on your boards to connect with uniflash for formatting and updating the service pack and user files.
Regards, Ankur
Thanks ,
Victoria