Hi all,
I have made a prototype with a CC3200R1M2 supplied by TI.
For to program it, I use a part of the CC3200 LAUCHXL :
GPIO1 and GPIO2 of my own board are connected to J7(3) and J6(3) of the LXL.
Reset is connected to LXL P2.5 and so on.
I disconnect th CC3200 of the LXL removing J12.
SOP2 is 1,SOP1 is 0 and SOP0 is 0
I have tried to communicate with my board using CCS UNIFLASH but it doesn't work.
Making the hypothesis that my board is OK, is there something wrong on my approach ?
Are the CC3200R1M2 ready to work with the good bootloader ?
Thanks for your answer.
Joseph TORRENTE