I'm trying to build a system with multiple tasks on a CC3200 lauchpad board with freeRTOS. I created three tasks in my main (based on the freertos demo)
All three tasks have the same priority (1) and therefore I expect that all three tasks will get the same amount of processor time.
Each task is only responsible for printing its name on the uart port:Unfortunately, I only see the highest priority task printing its name all the time and in the case that the priorities are equal I receive a faulty interrupt. What should I do to fix this?