I am using CC3200-LAUNCHXL with CC3200AUDBOOST and CCS 6.1.0
In SDK 1.0.0, wifi_audio_app seemed to work.
In SDK 1.1.0, it doesn't even blink the LEDs.
Is this problem familiar? Solved?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am using CC3200-LAUNCHXL with CC3200AUDBOOST and CCS 6.1.0
In SDK 1.0.0, wifi_audio_app seemed to work.
In SDK 1.1.0, it doesn't even blink the LEDs.
Is this problem familiar? Solved?
Hi Oshry,
In current version LED indication is off as same PIN 1 and 2 are used for I2C(Audio codec). In last version version we were enabling PIN 1 and 2 as GPIO once codec configuration is done over I2C(see comment line#330 in main.c ). As we added volume control feature that need access to audio codec all time that's the reason LED indication are disable. If you don't want to access audio codec once its configured please uncomment line#320, 321, 326, and 327 in main.c
Regards,
Aashish