Hi
I am try to connect the mqtt client with security, i found the struct SlMqttServer_t with following defined, what is that mean the field "method" and "cipher", i can not found their definition. thank you
typedef struct {
#define SL_MQTT_NETCONN_IP6 0x04 /**< Assert for IPv6 connection, otherwise IPv4 */
#define SL_MQTT_NETCONN_URL 0x08 /**< Server address is an URL and not IP address */
#define SL_MQTT_NETCONN_SEC 0x10 /**< Connection to server must be secure (TLS) */
_u32 netconn_flags; /**< Enumerate connection type */
const char *server_addr; /**< Server Address: URL or IP */
_u16 port_number; /**< Port number of MQTT server */
char method; /**< Method to tcp secured socket */
_u32 cipher; /**< Cipher to tcp secured socket */
_u32 n_files; /**< Number of files for secure transfer */
char * const *secure_files; /* SL needs 4 files*/
} SlMqttServer_t;