Hello again!
I'm working with a CC3200 Launchpad, creating something like an "UART/I2C to TCP/IP Converter". The board is in Station mode: there's a TCP server stack, an UDP stack (for something like mDNS) and a HTTP server too (just to inform the IPs for the user). Everything is quite fine, but I have some questions to make it (almost) perfect!
- When the board is in DHCP mode, how can I get the acquired subnet mask? (looks like there's no entry in SL_NETAPP_IPV4_IPACQUIRED_EVENT);
- In scan policy, what's the RSSI range? (maybe -40 to -87 dBm?);
- About scan policy, is it possible to do a new scan when the board is already connected to an AP (and without lose this connection)? If not, can I only read the actual RSSI of the connected AP? (to use in HTML, for example, so the user can move the board to get a better position);
- In station mode, is there a way to access the HTTP server by a hostname? (I don't think so, maybe I need a NetBIOS stack, using that URN field as a hostname...);
- About TCP server socket, how can I know if the client disconnected from the server? (after sl_Accept, my stack waits for anything with sl_Recv function).
Thanks for your attention!