Dear Uniflash users,
New Uniflash version for SimpleLinkTM CC31xx/CC32xx is now available for use.
Please note that up to version 3.2.0.000123, support for SimpleLinkTM CC31xx/CC32xx devices was not part of the Uniflash main stream where all other platforms are supported. However, now that Uniflash has been upgraded to v3.3.x, SimpleLinkTM CC31xx/CC32xx is also included as one of the supported chipsets. To prevent confusion, v3.2.x is also updated to align with v3.3.x.
The new version is 3.2.1.00000 for the 3.2.x standalone or 3.3.0.00058 for the 3.3.x mainline. The new version should be available soon on http://www.ti.com/tool/uniflash. Meanwhile, 3.3.0.00058 can be downloaded from the following WiKi page http://processors.wiki.ti.com/index.php/Category:CCS_UniFlash#Download_the_Latest_UniFlash_Web_Installer
The new version mainly offers Image Programming support and automatic reset when connected to TI EVB (as well as some bug fixes).
For further reading please refer to 'Image Creation and Programming' chapter in Uniflash User Guide. It can be found in the following link:
http://processors.wiki.ti.com/index.php/CC31xx_%26_CC32xx_UniFlash
Good luck