Hi,
Wi-Fi applications based on the TI SimpleLink Wi-Fi CC3100 and CC3200 solutions use a serial flash memory for non-volatile storage. It was previously suggested that TI’s CC3100/CC3200 devices could be used with the Micron M25PX80 8 Mbit serial flash. TI has recently been informed by Micron that the M25PX80 8 Mbit serial flash will soon transition to an end of life status. In addition, based on further recent stress testing in TI labs, we have found that pending accesses to the serial flash may not complete correctly in all situations when the power supply is turned off. This can result in possible data corruption issues when using this particular serial flash.
Recommended actions to achieve optimal performance
Systems using the SimpleLink Wi-Fi CC3200 or CC3100 solutions with Micron M25PX80 8 Mbit serial flash should transition as soon as possible to the footprint compatible Winbond W25Q80BL 8 Mbit serial flash or the Macronix MX25V8006E 8 Mbit serial flash.
For additional details, please visit Serial Flash Application Note:
http://processors.wiki.ti.com/index.php/CC3100-CC3200-SFlash-Recommendations