We're using a third party company's WIFI module using CC3220 chip, and use SimpleLink technology to set CC3200's wifi password. We've developed an app base on SimpleLink Wifi Starter. However, the connection is very unstable. The app can't match device easily. According to the third party company's explanation, TI C3200 chip's SDK only support 32bit iOS app, and doesn't support 64bit iOS app. Does anyone else encounter the same problem as I did? I only found there is SmartConfig iOS SDK 32bit and 64bit support for CC3000.