Can the CC1111 USB RF access point from eZ430-Chronos be use as Capture device for SmartRF Protocol Packet Sniffer?

Can the CC1111 USB RF access point from eZ430-Chronos be use as Capture device for SmartRF Protocol Packet Sniffer?

the eZ430-Chronos page http://processors.wiki.ti.com/index.php?title=EZ430-Chronos#Compatible_RF_Development_Boards "CC1111EMK868-915 CC1111 868/915 MHz Evaluation Module. This is similar to the USB Chronos Access Point except for minor differences in the schematic. It also includes additional headers and for reprogramming using the CC Debugger. "

10 Replies