I would like to ask if the final average limit is deduce by equation a) or equation b)?? . Our device was set to 100% duty cycle during testing.
a) Final average value = Measured Peak value + 20log(duty cycle)
b) Final average value = Measured Average value + 20log(duty cycle)
Which one is correct?
I have check a test report from Ember, they use equation b).
http://ember.com/faq/files/EH0533-2_EM260_RCM_Report.pdf
http://ember.com/faq/fcc-certification
However, our local test lab (SGS) said the calculation should base on equation a). The lab tested the device with both peak detector and average detector.
Now, i have some problems with CC2530 that we over the limit for 2dB in the average value at 3rd harmonics. I calculate our worst duty cycle is about 17ms/100ms = -15dB.
If DCF is applied for equation b), i have no problem in releasing the product at all. If not, gotta to redesign the product. :((
Please see if anyone can give me some advise ......