1106.PSD_2_PCAP_Convert 1.0.0.zip
While working on a project, I put together a C++ program to convert files that are outputted from the TI Packet Sniffer program in PSD format to the PCAP format that can be used with Wireshark. I thought it might be useful to others, so I'm posting it here along with the source code under GNU General Public License. Functionality is pretty basic at this point and it runs on the command line.
Usage: PSD_2_PCAP_Convert <source PSD file> <destination PCAP file>
It has been tested under Windows XP and Windows 7 with output from the CC2531DK USB Dongle and seems to work. The only thing that appears to be lost is the packet checksum, which appears to have been replaced with signal strength info from the Sniffer program.
Hope it helps someone else out there,
Torrey Bievenour
Vision Quest Lighting, Inc.