hi
we are trying to use packet sniffer to monitor sub ghz 802.15.4 star network with cc1310 chip.
the setup is based on ti 15.4 stack example with beagle bone black + collecor firmware on cc1310 launch xl + sensor firmware on cc1310 xl
that setup above works fine.
i installed packet sniffer 2 and wireshark correctly then programmed sniffer_fw_gfsk_50kbps_868_915.hex file another launchxl_1310
but when i try to configure radio from packet sniffer 2 it only allows to set frequency 863.125 mhz on 868 mhz band. since"868.0–868.6 MHz: Europe, allows one communication channel "
that 863.125 mhz does not looking correct ? also the sniffer not getting any packet from air beside network is working correctly. so i am sure there are valid packets on the air.
any idea ?