Tool/software: Code Composer Studio
Hi,
I am using CC2640R2 launchpad as debugger to load and debug program in custom board.
My CCS version is 7.2.0.00013 and i am using simplelink sdk 1.35.
Before a few weeks ago, i can debug the program very well.
At the beginning of this week, i was getting errors and ı am nearly unable to debug the code.
I used same custom board and debugger for all time.
When i press the Debug button, i got the following errors.
Cortex_M3_0: File Loader: Memory write failed: Timed out waiting for target flashloader to execute command.
Cortex_M3_0: GEL: File: deneme.out: Load failed.
When i got these errors, i am doing these steps to load program to board and debug.
- View/Target Configurations
- Opening CC2640R2F.ccxml
- Selecting advanced option on the bottom line
- Clicking the CC2640R2F in All connections panel
- Then, press debug
- Right click on Texas Instruments XDS110 USB Debug and click the connect the target in Debug panel as shown in pciture
- Press Load button on the upper panel and select the firmware to load
- Loaded successfully.
I inserted breakpoint to program.
Cortex_M3_0: JTAG Communication Error: (Error -1170 @ 0x0) Unable to access the DAP. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK). (Emulation package 6.0.628.3)
I got these error so much and so frequently. This is also happening TI provided examples.
I tried with disabling POWER_SAVING. However, nothing changes.
I am open to any suggestion and help.
Thanks for your attention