This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

CC2640R2F: CC2640R2F无法下载程序,各位帮忙看下

Part Number: CC2640R2F
Other Parts Discussed in Thread: CC2640

各位朋友,帮忙看下分析下原因。
如题CC2640R2F不能下载程序,SmartRF Flash Progarmnmer 2 不能识别我的板子,但能识别XDS100V3下载器;
具体情况如下图所示:

错误230,按照论坛给出的解决方案,擦除CC2640的FLASH ,显示擦除失败。

1、说明一下:CC2640R2F的引脚DCDC_SW已经输出了1.6V了,是正常的。但板子上的24MHz晶振不能起振。。。
我现在怀疑是下载器的问题了。我的板子原理图如下图所示:

我的板子是按照TI官方的开发板绘制的,官方原理图见附件:

LAUNCHXL-CC2640R2_1_0_0_Schematics.pdf

2、说一下我使用的下载器,是在淘宝上买的一个XDS100V3下载器,用来给我的CC2640R2F板子下载程序的。
按照淘宝卖家发给的资料(资料差的可以,都是N年前的破资料),就一张图片对我有用。。  

3、下载器与我的板子连线如下所示:这些连线,我用万用表都测量好几遍了,是正常连接的。
XDS100V3下载器         CC2640R2F板子下载口
(1)TMS--------------WMCU_TMS
(5)PD---------------V_3.3V
(11)TCK------------WMCU_TCK
(15)SRST_N-------WMCU_RESET
(4)GND.1----------GND
(8)GND.2----------GND

4、我的板子上CC2640的下载接口如下图所示:

  • Note that the language used on E2E is english.

    I ran part of your text through google translate and have a couple of questions:

    - You wrote something about the xtal not starting, how do you know this? Note that the xtal typically only is used when needed, meaning that when trying to connect to the debugger the chip is running off the internal RC OSC.

    - Do you know that the XDS probe you got supports the CC2640R2F?

    You can try with the XDS110 on the launchpads and see if you manage to connect with that. 

  • 谢谢回复。抱歉,英语比较差,望理解。关于此问题我已经解决了。

    由于不确定从淘宝上购买的XDS100V3下载器是否支持CC2640R2F,所以我将下载器退货了。
    然后7月9号从贸泽上贪便宜买了一块cc2640R2F LanuchPad的开发板(只需要227RMB,淘宝上最便宜的也需要235RMB)。
    本来大概需要一个星期能收到货的,坑爹的是被海关扣押检查了一个星期;
    导致7月21号才收到货。


    官方的CC2640R2F LaunchPad,上电之后测量CC2640R2F的引脚DCDC_SW点的电压为1.67V,DCOUPL电压为1.27V;

    我刚开始以为我的板子DCDC_SW点的电压已经为1.6V,芯片焊接应该没问题了;
    可是使用TI的CC2640R2F LaunchPad板子自带的xds110下载器,仍然不能给我的的CC2640R2F下载程序;

    后来又重新将芯片焊接了一遍;再次测量DCDC_SW点的电压,这次为1.67V,DCOUPL电压为1.27V;

    然后程序就下载成功了。

    重点:从上可得知,当CC2640R2F芯片使用内部稳压器件,DCDC_SW输出电压必须是1.67V,DCOUPL电压必须为1.27V;

  • I suggest you to share your experiences in Chinese E2E forum to benefit other in China.