• Resolved

Can I use TRF7970AEVM to read/write mifare plus?

I have a project use TRF7970A.

But I don't know how to do read  mifare plus cards.

Please help.

Sem

// 5) { sendMessage("gtbTranslateLibReady", {"gtbTranslateError" : true}); return; } setTimeout(checkLibReady, 100);}gtbTranslateOnElementLoaded = function () { lib = google.translate.TranslateService({}); sendMessage("{EVT_LOADED}", {}, []); var data = document.getElementById("gtbTranslateElementCode"); data.addEventListener("gtbTranslate", onTranslateRequest, true); data.addEventListener("gtbTranslateCheckReady", onCheckReady, true); data.addEventListener("gtbTranslateRevert", onRevert, true); checkLibReady();};function onCheckReady() { var ready = lib.isAvailable(); sendMessage("gtbTranslateLibReady", {"gtbTranslateError" : !ready});}function onTranslateRequest() { var data = document.getElementById("gtbTranslateElementCode"); var orig = data.getAttribute("gtbOriginalLang"); var target = data.getAttribute("gtbTargetLang"); lib.translatePage(orig, target, onProgress);}function onProgress(progress, opt_finished, opt_error) { sendMessage("gtbTranslateOnProgress", {"gtbTranslateProgress" : progress, "gtbTranslateFinished" : opt_finished, "gtbTranslateError" : opt_error});}function onRevert() { lib.restore();}})(); (function(){var d=window,e=document,f=".",g="UTF-8",h="complete",i="head",j="link",k="script",l="stylesheet",m="text/css",n="text/javascript";Math.floor(2147483648*Math.random()).toString(36);function o(b){var a=e.getElementsByTagName(i)[0];a||(a=e.body.parentNode.appendChild(e.createElement(i)));a.appendChild(b)}function _loadJs(b){var a=e.createElement(k);a.type=n;a.charset=g;a.src=b;o(a)}function _loadCss(b){var a=e.createElement(j);a.type=m;a.rel=l;a.charset=g;a.href=b;o(a)}function _isNS(b){for(var b=b.split(f),a=d,c=0;c
  • Sem -

    where are you stuck at? Mifare Plus cards are supposed to be backwards compatible with Mifare Classic - but question from this side would be which way/method are you wanting to use the cards. i can see that you have already been approved to download and have activated the Stellarisware version for the TRF7960 - so i will send you (i have your email already) latest version of the code we just finished for that which accomodates the -60/-60A and -70A (it looks at register 0x09 and configures SPI automatically for you)

    JDW

     

    BR-

    Josh

    ---------------------------------------------------------------------------------------------------------
    Please click the Verify Answer
    button on this post if it answers your question.
    ---------------------------------------------------------------------------------------------------------

  • In reply to Josh Wyatt:

    Dear Nr Josh

    I am now in decelopment process for a proyect that needs to use mifare tags   with the TRF7979   . I have the same problem with mifare tags in the TRF7970  as some of your previous e-mails  have you some source to  evaluate  and some  exe file or script  to evaluate with the  TRF7970EVM  . In addition , there are any place where I  can find the code source for the GUI of the evm

    Many tanks

    Manuel

  • In reply to Manuel Lopez Palma101332:

    Manuel -

    Here is the GUI source code for the TRF EVM.

    http://www.ti.com/litv/zip/sloc135

    If you need the Mifare specific one, let me know. josh.wyatt@ti.com

     

    BR-

    Josh

    ---------------------------------------------------------------------------------------------------------
    Please click the Verify Answer
    button on this post if it answers your question.
    ---------------------------------------------------------------------------------------------------------

  • In reply to Josh Wyatt:

    Hi Josh,

    Please share this code with me please.

    Thank you