Hello,
I got an TRF7960A EVM which worked just fine.
But after downloading the TRF7960A C Code Samples
(ZIP, 153 KB) 309 views, 10 Aug 2011
without any changes to it the EVM stop working. Which means I get timeouts when I try to connect it to the GUI. And in stand_alone it stays in
while(irq_flag == 0x00)
{
} // wait for interrupt
How can I get back the original firmware (if possible plus code) ?