TRF7960A works on 5V full power output and connected external PA(4W) and external big antenna, RFID software is based on new firmware, How many tags can TRF7960A read?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Brian,
No worries. I was provided a couple slides which may help you understand the range limitations and the impact that multiple tags can have in the RF field: HF Tag Read Ranges.pdf
Regarding the issue you found, I don't think I quite understand the orientation you described. Can you send a picture of the tag location and antenna location so we can try and figure out if this is an RF issue or firmware issue?
Hi Ralph,
Thanks for sharing these relation curve figures of read range with me, it is very helpful to analyze my application.
I flatted these tags at random on the antenna plane like the following picture, two kinds of problems can occur:
1. Reader stopped to detect tags; (can not see SPI/IRQ signals output on scope)
2. Reader is detecting tags, but can not get any tags UID or data. (can see SPI/IRQ signals output on scope)
Thanks.
Best Regards,
Brian
better check your antenna tuning and Q first - you should have no trouble reading those (if they are full size cards) how big is the antenna? what is the tuning and Q of it?
Hi Ralph,
The antenna's Q value is about 50, sorry, they did not reply me it's work frequency deviation.
For stack, I did not see software crash on uVison, it seems that it can not be stack overflow issue, it is pending on SPI writing because of SPI controller has been busy all the time.
Both (NO_RESPONSE_RECEIVED_15693 and NO_RESPONSE_RECEIVED) are used, it can went into the two status of TRF796X when running separately. there is 6ms time between them.
Thanks.
Best Regards
Brian
Hi Ralph,
I have not considered Q value and tuning of antenna yet, and I have not instrument to measure them now, Could you tell me how can I determine Q and tuning? then I can customize right antennas from the provider.
If bad Q and tuning is used, can firmware detect this case to handle it?
For what you asked, there is 6ms time between turning the RF field on for the TRF7960A and sending out the anticollision command?"
NO_RESPONSE_RECEIVED_15693 interrupt is used in anticollision handling in code. what is the difference between NO_RESPONSE_RECEIVED and NO_RESPONSE_RECEIVED_15693?
Thanks
Best Regards
Brian
Hi Ralph,
For ISO15693,BW is 846kHz when one subcarrier is used and Q is about 16, Is it right if I select this Q value?
Thank you for your clear description for two TRF796X status.
But sometimes there is some problem on SPI writing, it seems that SPI work is not stable, CMU SPI are connected to two devices(TRF7960 and EEPROM), Can it be SPI hardware design issue?
Thanks
Best Regards,
Brian
Hi Ralph,Who can I ask some problem about TI HF power amplifier reference board?
Thanks.
Best Regards,
Brian
Hi Ralph,
Ok, can I use your design totally and only remove auto bias?
Thanks.
Best Regards
Brian
Hi Brian,
I recommend using the updated amplifier design attached. TRF7970 Exernal Power Amplifier for general applications_V53(1).pdf
Hi Eddie,
Thank you so much for sharing this with me, it is very helpful for continuing my design. I will take some time to understand this and come back to you.
Thanks
Best Regards,
Brian