Hi, I want to buy a TRF7960A Evaluation Module. But I have a problem. It says it supports for the ISO 15693 standard, the ISO 14443A standard and the ISO 14443B standard. Does it mean it can communicate with any RFID tag supporting the same protocol? Such as, does it support the MLX90129 Sensor Tag / Datalogger IC from the MELEXIS ? I have the MLX90129 datalogger IC, and it supports the ISO 15693 standard. Waiting for your reply. Thanks!