Hey, i bought a PaLFI kit and i intended to greatly increase read range, therefore i bought a RFM-007B RF High Power Module to increase read range and two antennas G01E Antennas to double it. Then i realized by mistake that two 27uH G01E Antennas in parallel wont work with this standard RF module. In this case, i would need two 54uH Antennas in parallel to appear as a 27uH single antenna.
Any idea how to solve this problem, in order to use this module and these two gate antennas together?