Hello,
We have designed an RFID reader device by using TRF7970A and MSP430G2553 and a PCB antenna whose dimension is 50mm*40mm.
Power supply for the system is 3.3V and hence the maximum RF power output we expect is 70mW (Correct me if it is wrong). We are using the TI tags, Tag-it HF-I plus transponders (ISO 15693 protocol).
With these configurations, we are able to read the tags at a distance of 8 to 9 cms whereas, we are having a requirement for 25-30 cms of reading distance. As we are looking at a miniaturised product, we couldn't increase the size of the antenna which can help in increasing the reading distance.
Can you please suggest us any solution regarding this requirement?
Note: We came across an application note from TI which is using TRF7960 and multiple antenna boards multiplexed to the single reader. Can this be a potential idea for us to go forward?
Thank you.
Regards,
Maddineni