I have a board with a TRF 7970A chip with a firmware that is the same as TI EVM. When running the TI TRF7970 EVM Control app from the 14443A Tab, with a RFID Tag NTAG 213 from NXP, the Anticollision commands returns the UID, but after the Select command is sent, the response is not as expected:
12:21:53.437 --> 0109000304A0010000
12:21:53.593 <-- 0109000304A0010000
14443A REQA.
(04)[0466A04A52623E808E]
12:22:14.976 --> 0111000304A20466A04A52623E808E0000
12:22:15.133 <-- 0111000304A20466A04A52623E808E0000
14443A Select.
(4400)(04)[00]
The format according the slou321.pdf should be:
(xxxx)[yy]
Does it mean that the current firmware in the board is not compatible with the RFID Tag?
When sending the the command 010A0003047230110000 (read 4 blocks from address 0x11)
the response is :
13:16:46.059 --> 010A0003047230110000
13:16:46.180 <-- 010A0003047230110000
NFC Type 2 command
[NACK]
Is there a solution that will allow to communicate with the RFID Tag?
Thanks