Hello Everyone,
I've recently took over support for a RFID reader that utilizes the RI-R6C-001A (S6700 Multi Protocol Transceiver IC) to manage ISO/IEC 15693 smart tags. The reader generates a write single block command to the tag and the write is successful. However, the transceiver IC doesn't signal reception of the command response to the micro-controller. Now, the current firmware is disabling the Manchester Decoder in the transceiver command, but there is no comment or documentation on the reason the decoder was disabled. The firmware is handling the Manchester Decode as long as it can identify a good Start-Of-Frame (SOF), but I'm seeing cases where there is NO discernable SOF from the transceiver. I've sought the errata for the IC,but so far I've found no errata on the TI web-site.
Thanks,
Gerald Stanton