Hi, I am in the process of developing a system based around the TRF7970A and need to match my PCB coil to 50ohm. I believe I know how to do this using sloa135 for reference.
In sloa135a the desired quality factor is 6.78 which makes since the target bandwidth is 2MHz in order not to block the 848k modulation.
I was looking at application circuit in the TRF7970A datasheet when some confusion arose... The circuit depicted there shows:
But if I use the equation for the quality factor of the inductor with parallel resistor (same equation used in sloa135a) I get:
Q = Rp/XL = (6800)/(2*pi*13.56*1.5) = 53.3...
Isn't a quality factor of 53 too high for the application? I saw that 8-10 was recommended in a previous thread
Also, when I used smith chart to find the input impedance to the coil + matching (after R2) I get about 36 ohms instead of 50. Is this correct?
Thanks,
Eric Horton