hi,
i have a question concerning the 3 internal regulators of the TRF7970 (VDD_X, VDD_RF, VDD_PA).
in the datasheet it is noted that the 3 regulators turn on after EN pin goes high. (EN2 pin is on ground; VIN=3.3V)
now i noticed in my circuit that only VDD_X and VDD_A turn of after EN -> high but VDD_RF turns on immediately after there is voltage supplied on the VIN pin.
è Do you know if this is normal or what the problem could be?
è Because I want that all 3 regulators turn on after EN -> high
thanks a lot
regards
chris