I've been using TMS3705 for almost 6 to 7 years with the very same circuit.
I'm facing a problem that has appeared after about 20 days of full operation.
The response time (when TXCT goes high after the charge time) is usually within 20ms, but after these 20 days of operation the response time is now random. Sometimes I can get a response within 20ms, but most of the times now I'm getting a time bigger than 20ms. Sometimes is 200ms, 400ms or even 800ms.
I can't hold my system waiting 800ms for TMS3705 to deliver the ID.
I'm suspecting the power supply, because TMS is being supplied by a boost step-up with 5.5V since it's battery powered.
According to the datasheet 5.5V is the maximum recommended voltage.
Could this be the problems?
Help please.