Hi,
I'm developed a board with trf7970a according to the eval board and its connected to a cpu.
First I set the spi Cs to hight, 5ms delay and set the trf7970a EN pin to high (en and en2 pulled via 10k to gnd).
Band gap measured 1.6V, sys_clk is 3.38 MHz, the supply voltage is 5V, the 13.56 MHz osc measured and its fine.
I tried allready two pcb's.
The oscilloscpe is conneted to the irq and on this pin an interrupt is set with a ++ variable but I do not detect any interrupt.
Do you have any idea what can be the problem?
Best Regards,
GH