Other Parts Discussed in Thread: MSP-FET
Tool/software: Code Composer Studio
I have a
Battery-less NFC/RFID Temperature Sensing Patch
and want to reprogram it for doing experimental custom temperature sensing. On the RF430FRL152hEVM there is a complex MSP-FET to RF430 circuit that connects the FET voltage (3.3V) to the EVM voltage (1.5V) Since the patch doesn't have this circuit, where can I get a voltage convetor the goes between the patch and the FET? There are testpoints that I assume would allow such a thing.