Part Number: MSP-EXP430G2
Hello,
I have the msp-exp430g2 ( Revision 1.5) and DLP-7970ABP.
I have programmed the mcu ( msp430g2553) via Uniflash with the TRF7970ABP_RFID_Reader_Demo.out file.
I cant read the data through the docklight in spite of doing the right parameters in the com's. ( Like Flow control Hardware, Baud Rate 9600..)
I have tried to connect the mcu with an external usb to uart and i can get data.
What i have to do to get the same data with the on board usb in the launchpad?