Other Parts Discussed in Thread: MSP430FR5969, DLP-7970ABP
I am able to READ/Write into the NFC TAG 213, and now i am trying to do the same thing(READ/WRITING) with RFID(mifare) card. I am using MSP430FR5969 with TRF7970A module(SPI protocol).
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
I am able to READ/Write into the NFC TAG 213, and now i am trying to do the same thing(READ/WRITING) with RFID(mifare) card. I am using MSP430FR5969 with TRF7970A module(SPI protocol).
Hello Anil,
The MIFARE Classic example for the TRF7970A is: http://www.ti.com/lit/pdf/sloa214
This does not demonstrate tag writing, and does not run on the MSP430FR5969 though you can port the code. If you choose to make this port, I recommend getting a Logic State Analyzer so you can debug the timings and sequence of steps that are covered in great detail by the app note.
dear Ralph Jacobi,
void NFC_TYPE2_READ_4_BLOCKS(void); this predefined function is available on internet two read the data from NFC TAG, But i am not able to find any function to write/read from the RFID card.
and one more thing is that, i am using MSP430FR5969 with the TRF7970A module for interfacing with mifare cards for reading, so is this correct method or wrong?> or any predefined code is available to write and read. Please guide me.
hello ralph,
It is not mandatory to me to use only TRF7970A board, i can use the RFID_RC522(keystudio) board also for reading and writing, But for this one also i am not having any firmware("Embedded C" code). And i don't know about this board and is this board is OK for me or not?
I want to read/write some data into RFID(mifare) card anyhow. Requirment is only that use MSP430FR5969 and another supplementory module which is usefull to read/write into that. So any solution on this so please give me.
Thanks,
Anil D.