MIFARE Ultralight®, NTAG203, MIFARE Mini, MIFARE Classic® 1K, MIFARE Classic® 4K, FM11RF08
- what are the requirements to have our reader communicate with the Tag-it HFI-Plus?
Thank you!
Hans
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
MIFARE Ultralight®, NTAG203, MIFARE Mini, MIFARE Classic® 1K, MIFARE Classic® 4K, FM11RF08
Thank you!
Hans
Hello Hans,
Our Tag-It HF-I Plus transponders use ISO15693 technology for communication. Support of fundamental ISO15693 commands such as Inventory, Read and Write Single Block, and other functions which your end customer would like to implement in their system would be the basic requirements. If your RFID Reader only handles ISO14443A then it either doesn't support ISO15693 at a chip level (quite possible, single protocol chips are common esp. for ISO14443A) or you may need to enable that functionality via software.
I don't know what readers other charging station use, and even if I did it wouldn't necessary be okay for me to disclose that anyways.
Customers evaluating our tags typically also use our transceiver, the TRF7970A (or TRF7964A for Reader/Writer only as the 70A supports NFC modes like Peer to Peer and Card Emulation) as part of the evaluation, you can check our FAQ guide for basic details of these devices including recommended evaluation hardware and software: http://www.ti.com/lit/pdf/sloa246