Other Parts Discussed in Thread: MSP430F5529, , TRF7960
Tool/software: Code Composer Studio
Hi,
I tried to run an adapted version of the code given with the DLP-TRF7970A, to make it work with an TRF7960A associated with a MSP430F5529.
The thing is I don't have any response on the MISO port and the IRQ signal seems unusual.
I already changed the polarity of the serial clock on read/write direct command but as I followed the the application report on "Using SPI Interface with TRF7960",
I couldn't quite understand the next instruction about the IRQ Status Register Read, I tried to send the 0x6C command at each command sent but I had no more RF output after making that change.
Also, does the fact that the FIFO in the 60A is 12-bytes long and not 127-bytes long interfere with the reading protocol ?
Here a pic on the signals that I obtain :
Blue : IRQ
Red : RF output
Green : MOSI
Yellow :MISO
Regards,
Samy