Hi. We would like to use TRPGR30ATGC transponder by placing it inside a plastic container and hanging on a small animal's stainless steel collar. I have a few questions. First, will a sub-centimeter proximity to metal still let us read the tag? Then, if the dirt or urine get inside the container with the glass encapsulated tag, will this interfere with the tag's detection? Also, can the tag be read in proximity to regular power supplies/ computer monitors? And finally, if there is a scratch on the glass surrounding the tag, can we still use it? In other words, how bad the damage should be to stop using the tag? Many thanks for your help.